This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: MONx noise

Part Number: UCD9090A
Other Parts Discussed in Thread: OPA2333,

My customer is driving the MON1 pin with an op-amp at 0.56V. It is an OPA2333 micropower op amp. They are seeing a noise transient on the op-amp output (MON1 pin) at around 100mV with a frequency of ~130KHz. They are using MON1-7, MON8-11 are unused. There is no external capacitance on the MON1 pin to GND. Feedback resistance around the op-amp is 10K ohms.

Is it possible that the internal UCD9090A MUX is introducing this noise on the MON1 pin? Any other thoughts about what might be causing this- it does not correlate to anything in or around the op-amp. Everything is very clean.

Thanks, Mark