Hi,
I would like to use UCD9090A for power up/down sequencing.
Since UCD9090A is controlling all the CPU power on our board power-up sequencing shall start when main power rail (rail #9) is on.
Due to auto-on, I cannot use OPERATION or CONTROL mode, since the CPU cannot issue command or trigger the control pin yet.
Power off sequencing shall start, when power good off or undervoltage condition occurs on rail #9, but soft-off mode is not supported by Fusion GUI.
In chapter 4.7 of SLUA815 it is stated, that either using fault response to start sequence down or usage of pin selected state feature.
Is it recommended to define a GPO that indicates power good of rail #9 and use that to drive CONTROL pin?
Alternatively what else can be down to have both power up and down sequencing based on the voltage level on rail #9?
Thank you in advance.
Best regards,
Peter