This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160A: BPCAP & V33A Connections

Part Number: UCD90160A

We find the following references doc. differences for the BPCAP and V33A pin connections:

1.) V33A:

    a.) Data-Sheet pg 48 & Schematic Guidelines (SLVUB50) Pg 2: Connect to 4.99 ohm resistor.

    b.) Evaluation Board (SLVU423) Pg 10: Connect to Ferrite Bead (220 ohms at 100MHz)

 

2.) BPCAP:

    a.) Data-Sheet Pg 48 & Evaluation Board (SLVU423) Pg 10: Connect to 0.1uF

    b.) Data-Sheet Pg 50, & Schematic Guidelines (SLVUB50) Pg2: Connect to 1.0uF.

 

Can you please help us reconcile these differences and advise on the correct connections to these pins?