Other Parts Discussed in Thread: LMZ14201, LMZ14203
Hello
I have now succeed to get the right flag sequence on my LM3880 thanks for the provided explanation.
I have another concern I try to command a LMZ14201 and 14202 , following the proposed schematic with the resistor divider
test result ( LM3880 is set with 100 K resistor ballast and works fine with LMZ connection )
LMZ14201 Vin is 12V
1) straight drive EN with a 5 V DC source that work
2) straight drive EN by using the LM3880 I destroy the LM3880
3) resistor divider ( 9.1K / 20K ) EN by using LM3880 = I do not succeed to drive the LM14201 I measure 1.2 V out of the LM3880 after the ballast
does someone can explain where is the problem ?
Thanks
David