Hello,
I have a problem with the Power Manager.
When I load a file to the Power Manager that runs perfect on other cards.
After loading the File into the Power Manager I make a reset to start the Power Manager new. But after the reset the Power Manager will not start the sequense.
But if I start the Fusion Desinger and the Fusion Desinger is searching for an available Power Manager, the sequense will satrt and the Power Manager works fine.
Do you have an idea why the PM not started after reset. In the Log Files there are no faults.
Thank for help
Christian Günther