This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps2660: TPS2660's EFT (IEC 61000-4-4) Spec

Part Number: tps2660

Hi.

I already knew TPS2600 is able to protect EFT. But I can not find detail specification.

Is it meet 2kV burst EFT spec?

Please let me know

1 Reply

  • Hi SS Jung,

    Yes, TPS2660 providies protection during EFT 2KV burst spec as per IEC 61000-4-4.

    Please place 1uF capacitor at the TPS2660 eFuse input.

    Regards,

    Kari.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.