This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPS2413: TPS2413 unexpected voltage

Part Number: TPS2413

I used the ORing Power Rail Controller (TPS2413) in 12V input ,the sch as follows,

When only 12V_1 is on ,The other power will have 2.5V Voltage ,which will drive the LED on .In

http://e2e.ti.com/support/power_management/power_interface/f/204/t/537301 , It’s said that it have leakage current from C to A of up to 10uA.  A small load on the front end of ~ 5.11k should be enough to bring to acceptable.

I tried 4.7K, the voltage drop to 2.2V,when I changed to 150K .A changed to -0.5V. I want to konw if my design changed to 150k ,will there any risks in my power-supply system?

  • Hi ,

    I have informed the appropriate engineer and he will get back to you soon.

    Best Regards,
    Rakesh

    --------------------------------------------------------------------------------------------------------

    To find the latest information on Power Switches, Visit www.ti.com/powerswitch 

  • In reply to Rakesh:

    Hi

    I am looking into this question, will get back by tomorrow.

    Regards,
    Kari.
  • In reply to Karikalan Selvaraj:

    any new developments?

  • In reply to Karikalan Selvaraj:

    HI
    Kari ,Have you reviewed this problem?
  • In reply to user5215821:

    Hi

    At 4.7k ohm at 'A', 2.2V is not expected. As per the measurements done (attached) by brian, 4.7k ohm shows about 4V.
    Do you have any other load on at the "A" side of ORing?

    In the meanwhile, let me take the measurements on EVM to confirm that at 150k, "A" is at -0.5V.

    Regards,
    Kari.
  • In reply to Karikalan Selvaraj:

    Hi

    I have check on the EVM.

    With 5K at A, I measure 4.6V, --> this means 0.92mA current.

    With 150k at A, I measure 10.0V --> this means 0.066mA current.

    This is consistent with attached measurement from the E2E thread

    ""

    Attached the results here again for reference.

    TPS241x Leakage Path_Measurements.pdf

    By any chance do yo have additional resistance path on A, coming in parallel?

    Regards,

    Kari.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.