Hi support team.
My customer is evaluating a TPS25944A at EVM.
I received a question from him about Ton(dly) and Toff(dly) which are 220us(tpy) and 2us(tpy) on datesheet.
He got the result of Ton(dly) /Toff(dly) are more longer/shorter than datesheet spec.
(Please refer to attached .docx file.)
He thinks that his EN/UVLO setting is wrong.
His setting isthe below,
Vin=5V±10%
UVLO=4.58V
OVP=5.58V
R1=110kohm
R2=3.3kohm
R3=24.9kohm
(Above setting R1/2/3 is refered to datesheet on P22 Fig.50.)
If you can advise me, please let me know.Measured data Ton(dly)_Toff(dly) .docx
Best regards.