Other Parts Discussed in Thread: TPS22860
Hi,
I'm working on a design powered by CR2032 and I'm looking for a solution to increase life of my battery CR2032, and I'm wondering about using TPS22910A :
TPS22910 characteristics :
- active Low (ON input pin)
- RdsON is 61 mOhms
My device is always powered (80% to 90%) and sometimes not powered : is using these TPS22910 a good idea?
Currents are significant :
Device powered : Leakeage current + off supply # 0.2µA for Vin=3V
Device not powered : quiescent current #1.5µA for Vin=3V
Is the solution of using a P-MOSFET alone (FDN304P for example) is not better than the IC in these case?
Thanks for your help or any idea, design or IC to increase design efficiency
Best regards