Other Parts Discussed in Thread: TPS22965-Q1, TPS22918-Q1
Hi,
We got a question from customer about TPS22968-Q1.
Could you help us?
[Question]
Our customer considers to use load SW at below condition.
Vin=3.3V
Vbias=3.3V
Iout=2.5A
Vout rise time=5m to 6.6ms
They want the load SW which can be set high accuracy Vout rise time.
- According to TPS22968-Q1 datasheet figure 21, we can see the variation of tr is better than other IC such as TPS22965-Q1.
Is the variation of tr better than other products?
- Can the IC achieve their Vout rise time requirement? If it can't, is there any other products which achieve it?
- How can we estimate the tr at Vbias=3.3V? Could you give us equation at Vbias=3.3V?
Best Regards,
tateo