Hi Team,
Do we have p2p or same functaionality load switch solution to replace G5209AR1U?
Thanks,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi SHH,
We do not have any P2P devices which can work here. Can the customer accept a CSP device?
For 3.6V or lower, I would recommend the TPS22925C. The on-resistance is lower and the solution size is smaller.
For a 5V application, I would recommend the TPS22964C. The on-resistance is lower, the solution size is smaller, and the device has reverse current blocking.
If a plastic package is needed, the TPS22975 can be used. The on-resistance is lower and thermal shutdown protection is integrated.
Do you think any of these solutions can work?
Thanks,
Alek Kaknevicius