Other Parts Discussed in Thread: CC2650
Hi
I am facing problem with power switch TPS22960 output voltage zero for Input voltage 3.0 volt and ON1 and ON2 pin both are High (3.0V )
The voltage at VOut 1 is 2.5V and VOut 2 voltage is zero, it should be 3.0V or moe than 2.8V and less than 3.0V
Both ON1 and ON2 pins connected to GPIO pin of CC2650 and with 1K pullup resistor and CIN is more than CL
pls guide, what to do?
In big trouble on the final stage of project
See the schematic section
Please help