We use the TPS2115A in autoswitch mode and have connected two 5V0 power supplies to the device.
for VIN1 = 5.0V and VIN2 = 0.0V the output voltage is ~100mV
and
for VIN1 = 0.0V and VIN2 = 5.0V the output voltage is ~1000mV
My question is why is there an output voltage of 100mV or. 1000mV? I did expect that the output voltage is 0V
Best Regards
Patrick