Hi there,
first time poster. I've been advised that I need a load switch with under voltage cut off and hysteresis so that I can cut the connection to my load from the battery when battery voltage becomes too low and then reconnect the load when battery voltage has been charged to a higher/safer voltage.
Here are my details;
Solar MPPT controller charging battery and load connected in parallel, at night load drains battery, during daylight solar MPPT charge controller charges both battery and load.
I'd like some circuitry to control the connection from battery to load, during daylight allow load to be connected but when no voltage/current from MPPT and battery voltage drops to 2.8v cut off the load.
When battery gets charged up to say 4.0v allow load to be reconnected to circuit.
Is this possible with a TI product, can someone advise how this can be achieved?
Attached is a photo of set up I'd like to achieve.
Thanks,