This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2115A-Q1: Current consumption

Guru 16770 points
Part Number: TPS2115A-Q1

Hi

Our customer is requesting data about current consumption (min, typ, max) of TPS2115A-Q1.

Do you have it?

BestRegards

  • Hi na na78,

    We have a lot of supply and leakage current specs in the datasheet, and all typical numbers are already based on data we have taken during characterization for the device. What current spec is the customer concerned about?

    Thanks,

    Alek Kaknevicius

  • Hi Alek

    Thank you for your reply.

    They are asking supply current of blank part (min/typ) of the datasheet spec.

    - Supply current from IN1 (operating) in every test condition
    - Supply current from IN2 (operating) in every test condition
    - Supply current from IN1 (standby) in every test condition
    - Supply current from IN2 (standby) in every test condition

    The purpose of it is that they get the minimum, typican and maximum
    current consumption of load that connected to main source.

    If these data have not been exsisting unfortunately, it is OK. Please tell me accordingly.

    Then if possible, could you please tell us why min/typ data is not on the datasheet?

    BestRegards

  • Hi na na78,

    Since these devices were made over 10 years ago, we do not have a large amount of data to guarantee minimum or typical specs. In general, we do not usually list minimum values in our datasheets since we only test for the maximum values when testing the devices before shipment. For many of the currents that do not have typical numbers, the maximum is only 1uA, and this is already pretty low.

    For some of the typical values not listed in the datasheet, you can refer to the typical graphs (figures 10-13). 

    Thanks,

    Alek Kaknevicius