Hello,
I am using TPS26601 Industrial eFuse in one of our design. I am bit confused about the configuration of SHDN# Pin (Pin 14) . In the functional block diagram in Page 17 of Datasheet, it is clear that the pin is pulled up to a voltage Avdd through a resistor. But couldn't see the value of pull up resistor & the voltage of Avdd. Also in the specification at Page 5 the absolute maximum voltage of SHDN pin is 60 V and the recommended voltage is maximum 4V. What kind of clamping is used there ? ( Voltage ratings ? )
Can someone give an input on these ?
Thanks in advance.
Regards
Sreejith