This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

power mux

Hi.

I'm looking for a power mux that can handle two inputs automatic switching:

1. 4.5 - 17V, 4A max (adapter).

2. 3 - 4.2V, 4A max (Battery).  

The output should follow on the higher voltage input.


The output Current should be 4A max.

Can you please provide a suitable integrated solution?

BR,

 

Gilad.