Hi team,
Our customer have problem about TPS2115A.
Problem:
The drop voltage when shutting off the supply of 5 V is not improved even if measures are taken with the capacitor of the data sheet.
Is the following action possible?
IN1=5.0V -> 0V (USB unpluged)
IN2=3.0V
D0=Low
D1=High -> Low
OUT Voltage should transition from 5.0 V to 3.0 V without voltage drop.
thanks in advance.
Best Regards,
Kenji /Japan Disty