Dear Team,
One of our customer needs advises for a design of an e-fuse.
You can see below the requirements of the customer regarding his needs.
============================================================
"The need is to design an e-fuse on a bus of 11V, (since I do not have the right to exceed the 66% rating, I am at 7.2V) that opens the mosfet at 1 or 2 amps.
The problem is that it is necessary to cascade two in series in case of one is broken down. And the difficulty is : it must be very low consumption "
============================================================
Could you please advise us a device or topology that can meet these requirements.
Thank you very much for your help,
Best regards,