Hi guys,
One of our customers is considering using TPS2660 because the device is not broken even if VIN-GND voltage becomes a negative (reversed). But the customer has the following questions. Could you please give me your answers for the customer?
Q1. They want to use TPS2660 with /SHDN terminal pulled down by a resistor to GND. The /SHDN terminal is pulled up by push button or a output port of micro controller for TPS2660 activation. If VIN-GND voltage is reversed (becomes negative voltage) when /SHDN terminal pulled down by a resistor to GND, is the device broken or not broken?
Q2. /SHDN threshold voltage at falling edge is 0.76V(typ). What is /SHDN threshold voltage at rising edge? The typical voltage is 1.0V? Does /SHDN have any hysteresis voltage between rising and falling?
Q3. When I(/SHDN)=0uA, what voltage the /SHDN terminal voltage goes up to? Is it 4V as the maximum? Also what is Avdd voltage in the device block diagram?
Q4. On page 6 in the device datasheet, the following spec is shown.
LOW IQ SHUTDOWN (SHDN) INPUT
Parameter Test Conditions Min Typ Max Unit
V(SHDN) Output voltage I(SHDN) = 0.1 μA 2 2.7 3.4 V
I think the test condition, "I(SHDN) = 0.1 μA" is not correct and "I(SHDN) should be -0.1 μA. Is my understanding correct?
Your answer would be appreciated.
Best regards,
Kazuya Nakai.