Other Parts Discussed in Thread: TPS22912C, TPS22910A, TPS2113A, TPS2115A
In the process of designing a circuit for an app note and was wondering, is there anything wrong with using the TPS22976 as a simple way to OR two supplies? The datasheet says that both channels can be put in parallel but I'd prefer two inputs and one common output. This is a low current application (<100mA) and one of these ICs is way cheaper than two TPS2419s.
Thanks,
Carmen