Other Parts Discussed in Thread: TPS22918, TPS22975, TPS22958
I am using the TPS27081ADDCR device. I followed the configuration shown in Figure 13 Standard Application Diagram of the datasheet.
Part Values:
R1: 10K ohms
R2: 1K ohms
C1: 1uF
The load is a single 100uF capacitor
When I turn on the power, pin 4 VIN goes from 0V to 5V, pins 2,3 VOUT goes from 0V to about 2.2V even though pin 5, the ON/OFF is grounded. I would expect VOUT to stay at 0. This voltage then decays very slowly, about 4mV per second.
The device switches on as expected, VOUT going to 5V when pin 5 is pulled high.
Do you have any advice on why this device is always partially on?