LM74700-Q1 requires the GND pin to be connected. So, What is the suggested circuit for full-bridge rectifier using four LM74700-Q1? Or, LM74700-Q1 can only be used as the high-side controllers.
Any idea?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM74700-Q1 requires the GND pin to be connected. So, What is the suggested circuit for full-bridge rectifier using four LM74700-Q1? Or, LM74700-Q1 can only be used as the high-side controllers.
Any idea?
Hi Robert,
LM74700-Q1 has GND pin and this prevents use of this device for bridge rectifier applicaiton.
Regards,
Kari.