Other Parts Discussed in Thread: TPS2595
Hi,
I'm testing TPS2421 and i think that is working correctly. I tested Current Set, and TPS cuts at 2.85A, with RSET = 66k5 which means that my load is about 3R70. After this i increase the Load resistance and TPS just restarts at 1,80A which means 7R load resistance. From calculations that i send attached i see that resistive load at startup should be more than 12R, this is related to this or not?
Why TPS don't start after current is below ISET or why needs 12R at startup? In real environment is not possible remove the load at startup...
Best Regards1781.TPS2421_Design_Tool_Rev-.xls