Other Parts Discussed in Thread: LM74700-Q1
Hi everyone.
So I wanted to impelment LM74610-Q1 in my design but I am in dead end, I guess.
voltage applied to circuit is 18.5V. Maximum negative voltage of LM74610-Q1 is -45V.
This means that the TVS which is responsible for negative voltage spike suppresion should clamp voltage at 45-18.5 = 26.5V minimum.
Any TVS diodes that I look up which clamps at this voltage has working voltage of lower than 18.5V, which means it would start breakdown if voltage is applied with reverse polarity.
Is my only solution now to choose something like LM74700-Q1 or is there still some solution with LM74610-Q1 ?
Best regards,
Karlis Tucs