Hi,
I designing some device into aircraft and this part looks very usable for us, but I need know what is maximum working altitude for this part?
Thank you for answer.
Miroslav Pajpach
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I designing some device into aircraft and this part looks very usable for us, but I need know what is maximum working altitude for this part?
Thank you for answer.
Miroslav Pajpach
Hello,
this part is qualified for automotive environment and the ambient temperature is -40C to 125C. In aircraft and altitude, the environment is different in term of temperature and pressure. Inside the aircraft the pressure and and temperature may not change much from ground. If it was in the space outside the atmosphere, then there might be a concern.
Regards
Hello Mahmoud,
Thanks for your answer.
The device will be inside the aircraft, but outside temperature and pressure controlled area.
Maximal operating altitude is 50 000ft (15 200m) minimal pressure is about 11.7kPa. Still in atmosphere, not in space. But the environment will be much different. :-(
And additionally, with higher altitude, more (and stronger) cosmic rays are there.
So I need to know, where is a limit for this part.
I was unable to get firm answer. I believe we can not provide more info than the already provided.