Other Parts Discussed in Thread: TPS259230-41EVM
Hello,
I would like to use TPS25942A for single (18650) or double (2x16340) cell li-ion battery UV/OV/OC and reverse battery protection for a portable measurement product. The input voltage range is between about 3V (the low end of single cell) and 8.4V (the high end of 2-cell). The datasheet is well explained about UV/OV/OC protection. But for reverse battery protection, there is only very brief information in section 10.3.1.4 and Figure 86.
My questions regarding Figure 86 are:
1. Because the signal diode in the GND terminal path, would the input voltage shifted higher of Vf of the diode instead of 2.7 to 18V without the diode?
2. What impact of the calculation of UVLO, OV dVdT, ILIM, and IMON because of the signal diode in the GND terminal path?
3. Should the thermal pad of the chip be connected to the GND of the chip (pin16) then to the PCB ground plane through the signal diode, or connected to the PCB ground plane directly?
Thanks,
Danlin