Can we add different voltage to VCC and VAUXH with LM5064. Also it is not GND level.
Our customer is thinking the following using method.
Input rail: -48V
VCC: -35V
VAUXH: -41.2V (when input rail is -48V)
Please refer to the attached file for more information.
Is there no problem with such usage? Do you think that this circuit is more resistant to lightning surge?
Best Regards,
Kohei Sasaki