Other Parts Discussed in Thread: CSD19502Q5B
Hi all
Would you mind if we ask LM5069?
Please refer to the attachment file.
20180123_LM5069.pdf
Kind regards,
Hirotaka Matsumoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all
Would you mind if we ask LM5069?
Please refer to the attachment file.
20180123_LM5069.pdf
Kind regards,
Hirotaka Matsumoto
LM5069_Design_Calculator_REV_B per sch inputs needs work.xlsxHirotaka,
The design needs a lot of work. 1st FET selection: This Infineon FET is a poor choice for hotswap. It has extremly bad SOA, not suitable and may be too high Rdson depending on your operation current. Look at the CSD19502Q5B as a start. You may need even a stronger SOA than that. You need a much higher value dv-dt cap vs the 330pF. Timer is too short with 100pF. Go to www.ti.com/hotswap and download the design tools needed. There are excellent app notes and tutorial video on using the tools. I attached a 1st cut tool per the schematic. This should get you a start. Note the red items in the spreadsheet need to be corrected. You need to know the entire Cout downstream, not just what is on the schematic page sent, along with all of the system requirements.
Brian
Brian san
Thank you so much for your reply!
We got that customer's FET is not suitable, so we encourage the customer to change FET.
And then, we would like to confirm as follows;
・You need a much higher value dv-dt cap vs the 330pF.
・Timer is too short with 100pF.
By increasing Ctimer, it expands the minimum fault time (tflt).
There is the description on the datasheet "the minimum fault time (tflt) to be greater than the start time (tstart) by adding an additional margin of 50% of the fault time."
Does it mean tflt+margin > tstart?
And then, about dv-dt cap vs the 330pF, does it require to slow the rising time?
Kind regards,
Hirotaka Matsumoto
Brian san
And then, our customer changed Ctimer, after that they could solve the problem.
Thank you for your advice.
Kind regards,
Hirotaka Matsumoto