Other Parts Discussed in Thread: LM5069, CSD19502Q5B
Hello,
I need a fet controller for the below application but i'm not sure if the LM5060 would be a good fit. Recommendations on the controller and fet would be appreciated.
We are in need of a buck/boost controller with the following specs:
Output power : 600W
Input voltage: 24V
Output voltage: 20-29V
Regards,
David