I have posted the following threads in the past.
From the situation that the answer does not return, I felt be difficult the complianced of ISO7637-2@2004 seems to be severe with this device.
Therefore, I will try to consult about the below documents as reference with customers.
① If it is ISO 61000-4-5 (surge test), it can correspond under the following circuit diagram and VIN=24V, Load=16Ω.
②If ISO 61000-4-29 LV1 (Power Fail Test), it can correspond under the following circuit diagram and VIN=24V, Load=24Ω.
So check me my considering.
Can it permission to be "CLEAR status" will be performed if the same test is carried out according to the contents as described ?
Please also teach questions about ”TI design".
(Please tell me if it is another thread, I'll post it there.)
Is it possible to compliance Pulse 4 and 5a of 2004 version of ISO7637-2 when designing the circuit referring to the following documents?
http://www.ti.com/lit/ug/tiduc41/tiduc41.pdf
http://www.ti.com/lit/ug/tidub49/tidub49.pdf
Best regards,
Pokkun