Hello,
I have an application that will run at 56V nominal. The maximum recommended operating voltage is 55V. If I can guarantee that the input voltage of the TPS2660 will never exceed 60V, would this be an acceptable use case? Are there any concerns regarding product lifetime when operating at slightly beyond the maximum recommended voltage?
Don