I have designed a module for switching high current loads like 100A-200A using LM5060 and Mosfet in SOT-227 package (IXFN420N10T) and we have connected a resistive load of around 50A. At first, everything is powered off, then enable is set it opens up, but then its unable to close it anymore and stays always open. Gate to Source is 0.5 ohm and Gate to Drain is 22 ohm.
We use basic example schematic with added 0.01uF capacitor on the gate.
Any idea why this happens?