Hello
Would you please let me confirm the meaning about the note(2) on page 8 in the TPS4H160-q1 datasheet(Rev.c).
http://www.ti.com/lit/ds/symlink/tps4h160-q1.pdf
Is the meaning of note(2) correct as below?
"It is not meet to the current limit accuracy(±15%) on the datasheet until load current goes x1.5 larger than current limit setting."
if the meaning of above is correct, how is the minimum accuracy before load current goes x1.5 larger?
I worry about it limits on lower current than expected.
0474.TPS4H160_External current limit accuracy.pptx
for example,
Limit setting = 1A
actual curent = around 500mA
in this case, is there a possibility that the TPS4H160 limits at around 600mA or 700mA?
About Upper limit also,
Are there possibility that more than +15% load current flows continuously in case if it never reachs x1.5 larger than limit setting?
for example,
Limit setting = 1A , in this case, Are there possibility that 1.4A current flows continuously until once it reach 1.5A overshoot upper limit.
at last,
Would you please explain why it cannot meet tne accuracy in case load current once reach x1.5 larger?
my customer is developing ADAS application using TPS4H160 and mass production is 2018 August.
so, We need to clarify this problem soon. Please hepl us.
Best regards
Yamane