Other Parts Discussed in Thread: TPS2590
To avoid the start up current limit, im using a Mosfet after the output of the TPS2590 to switch on loads. When using a electronic load in constant resistance mode, this works fine. I can switch on 5A without problem. However, if i use the constant current mode, the TPS2590 switch off. Any idea what the issue could be?