Hello,
in one my project I just used TPS4H000-Q1 chip version B, that has 4 outputs at 1A max.
Now, my question is: can I connected 2 inputs and 2 output together in order to have 2 outputs at 2A? For example: IN1 and IN3 are input A and IN2 and IN4 are input B, then OUT1 and OUT3 are output A and OUT2 and OUT4 are output B.
Is it possible?
Thank You and Best Regards
Federico