This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

BQ51003: How to tune resonant capcitors value.

Part Number: BQ51003

Hello. 

I found a equation on bq510003 datasheet on page 27.  if use fs=10KHz, fd=1MHz, and Ls value is fixed. therefore C1, C2 will be worked out. 

But I use EVM parameter Ls=10uH to work out C1,  get C1= 3900000F. it doesn't match EVM C1=68nF + 68nF +47nF = 183nF. 

Could you please check it and give me a explaination. thank you!

Any side, I didn't find the equation on TX chip datasheet (bq50002A). how to work out TX resonant capcitors?  

  • Hello
    On data sheet page 27 equation 6 shows fs = 100kHz and fd = 1MHz. I do not see fs=10kHz.

    For C1 calculation the Ls' value should be used. This is measured with the coil mounted on a TX coil simulator , Fig 34.
    Ls' will be higher than free space inductance Ls used for calculation for C2 (Cd).

    For BQ51003 the Ls' value measured 13.5uH, this will calculate a value for C1 187nF, in the ckt C1/C2/C3 is 68nF/68nF/47nF = 183nF.

    The TX side is set by WPC standard for A11 TX. The L value is set at 6.3uH and resonant caps are set at 400nF.

    Best Regards,

    Bill Johns,  Applications Engineer

    Texas Instruments Inc

    Dallas, Texas

    Please click "This resolved my issue" button if this post answers your question.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.