• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » Wireless Power » Wireless Power Forum » difference between BQ51013EVM versions
Share
Wireless Power
  • Forum
  • Files
Options
  • Subscribe via RSS

difference between BQ51013EVM versions

difference between BQ51013EVM versions

This question is answered
Timothy Starr
Posted by Timothy Starr
on Aug 15 2012 08:01 AM
Expert1020 points

Hello

There are three versions of the BQ51013EVM, called -764, -65, and -725. All are described as exactly the same performance. Why are there three different versions? It would be nice if the differences were described somewhere, to help folks choose between them. Thanks and Best Regards,

-Tim Starr

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Rachel Coulter
    Posted by Rachel Coulter
    on Aug 15 2012 13:28 PM
    Intellectual865 points

    Tim,

    Thanks for the post. Hopefully this helps clear it up. It seems like the main differences between EVMs are packaging and being able to adjust certain features like charge status and Max Iout

    764

    765

    725

    WCSP layout

    QFM layout

    Not sure of package: possibly WCSP

    Multifunction NTC   and Control Pin for Temperature Monitoring, Done Charging and Fault Host   Control

     

    Multifunction NTC   and Control Pin for Temperature Monitoring, Done Charging and Fault Host   Control

     

     Single NTC/Control   Pin for Optimal Safety and I/O Between Host

     

     Programmable   Termination Pin for Charge Status 100% (CS100) Support

     

    Programmable   Termination Pin for Charge Status 100% (CS100) Support

     

    No mention of Programmable termination Pin

    Adjustable resistor R16 can be used to set max output   current

    Adjustable resistor R16 can be used to set max output   current

    No mention of adjustable resistor

    Includes these Pins:

    JP4 – Pull-Up to Out or Vz

    EN1 and EN2 pull-up along   with LED D1 can be powered from OUT or RECT. Vz is derived from RECT

    through a resistor and   zener diode.

    4.2.5 JP5 – CS100 TS Enable   or Disable

    Only used for bq51014   device. This jumper along with R14 and R13 will enable the Charge Status 100%

    feature. See data sheet for   additional info. Open will disable.

    4.2.6 JP6 – ILIM Fix or ADJ

    Max output current is set   by I-lim pin. In the FIX position current is set to 1.2A max. In the ADJ   position

    current is set by R16.

    Includes these Pins:

    JP4 – Pull-Up to Out or Vz

    EN1 and EN2 pull-up along   with LED D1 can be powered from OUT or RECT. Vz is derived from RECT

    through a resistor and   zener diode.

    4.2.5 JP5 – CS100 TS Enable   or Disable

    Only used for bq51014   device. This jumper along with R14 and R13 will enable the Charge Status 100%

    feature. See data sheet for   additional info. Open will disable.

    4.2.6 JP6 – ILIM Fix or ADJ

    Max output current is set   by I-lim pin. In the FIX position current is set to 1.2A max. In the ADJ   position

    current is set by R16.

    Does NOT include: JP4-JP6

    BQ51013EVM
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Timothy Starr
    Posted by Timothy Starr
    on Aug 16 2012 06:19 AM
    Expert1020 points

    Thanks Rachel

    That was a good answer...but I have an additional question. Are there any hooks for user dataq to be sent over the wireless comms link? Regards,

    -Tim

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Rachel Coulter
    Posted by Rachel Coulter
    on Aug 17 2012 11:24 AM
    Intellectual865 points

    Bill,

    I don't see much on user data for the EVM but here is some info from http://www.ti.com/lit/ds/symlink/bq51013.pdf on the bq51013 part and there is more info on communicatoin in the pdf.

    The receiver communicates with the transmitter by changing the load seen by the transmitter. This load variation results in a change in the transmitter coil current, which is measured and interpreted by a processor in the charging pad. The communication is digital - packets are transferred from the receiver to the transmitter. Differential Bi-phase encoding is used for the packets. The bit rate is 2-kbps.

    Various types of communication packets have been defined. These include identification and authentication packets, error packets, control packets, end power packets, and power usage packets. The transmitter coil stays powered off most of the time. It occasionally wakes up to see if a receiver is present. When a receiver authenticates itself to the transmitter, the transmiter will remain powered on. The receiver maintains full control over the power transfer using communication packets.

     

    Does this answer your question?

    Regards,

    Rachel

     

    bq51013
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Rachel Coulter
    Posted by Rachel Coulter
    on Aug 17 2012 13:57 PM
    Verified Answer
    Verified by Bill Johns
    Intellectual865 points

    Bill Johns was able to add additional information regarding your second question, Tim. Here is his answer:

    "No—Our bqTESLA products do not support Proprietary Packets at this time, customer specific data over the comm link."

     

    Thanks for your help Bill.

    Tim, I hope all the information helps.

    Rachel

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use