Can TI provide layout files (Gerber, etc) and schematics for this board? bq51050BEVM-764
Also, what value should Ros be?
-Jaden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can TI provide layout files (Gerber, etc) and schematics for this board? bq51050BEVM-764
Also, what value should Ros be?
-Jaden
Leonard,
When should Ros be used with the bq51050? And how do you compute it's value?
Thanks,
Ken
For design that does not need to comply with wpc1.1, the values on the EVM are good enough (200Ω and 42.2K). However, if the wpc 1.1 is need, FOD calibration is needed to find the right values of FOD and ROS.