I have an issue with a design using the bq51013A.
The following image is the output measured with an oscilloscope, when drawing about 0.5 A.
I'm using a Wurth 10 uH RX coil and I have a number of different Qi senders that I've used with similar result.
You can also quite clearly hear a high pithced sound that conforms well to the signal you see on the output.
I've used the following schematic, with the capacitors both as in the schematic, as well as with newer calculated values for 10 uH.
The newer values I use are C1=220 nF C2= 27 nF C3= 1 nF. C4 = 2400 pF C5= 160 pF. Both these values have been soldered on my PCB and both give more or less of this effect.
What strikes me as odd is that the bq51013AEVM HPA765 is specified with the capacitors I use in the above schematic, but from the equation in the data sheet of the bq51013A these values are way off.
In summary, my questions would be:
- Are my resonance calculations correct? (for L= 10.2 uH measured (or 10 uH on specs, not too big of a difference) I get C1 = 248 nF and C2 = 2.56 nF
- What can be done to minimize this effect, if it's not my resonance capacitor calculations that are off?