Hello,
I'm designing a battery charger complete with TX and RX using BQ500410A and BQ51050B for a lithium battery 2000mAh stylus.
I made the coil transmit and receive because they have to be small.
The charge cycle works this correctly, and it is of 800mA and interuptiona at 40mA .
What they do not understand is that when the charge current is between 140 and 400mA, during transmission from RX to TX, the charging current reverses the direction for some tens of mcroseconds.
As seen from the figure is the signal C1 is COMM1 and C2 is the current to the battery.
At the bottom you see the zoom and you can see the pulse of C2 at the beginning of COMM1 to 0 volts that go into the negative (current supplied by the battery)
I made 3 different layouts with capacitors as close as possible to the integrated circuit .On the RECT signal there are 2 10uF X7R and 0.1uF X7R 1, on BATT 1uF X7R, and 0.1uF X /7R.
When the current exceeds 400mA, there are no negative current pulses.
When the current drops below 140mA, in an instant, negative pulses of current disappear.