Dear TI,
I posted a couple of weeks ago the following schematic.
I used the EVM for the choice of the capacitors and the coil so i didn't tune it myself. For instance, I'm using the coil and capacitors recommended in the EVM. One is 9.7uH (IWAS 4832ff50) and the other coil is 10.5uH (WR48325015M2).
The ratings of the capacitors are 50 V.
My charging current is 100mA.
I am working with a Zens transmitter pad, Qi compliant.
http://www.makezens.com/shop/zens-single-wireless-charger-black/
but it doesn't seems to work.
I have the following measurement on RECT pin:
And in the COM1 pin:
I will make a new PCB and solder the components again. But i would like to know if there is something wrong in my schematic or measurements.
In addition I would like to know if you can guide me in the assembling of the PR1010. I am new in this wireless design and i can't understand Figure 3 in the Bq51050-EVM-764. How do i connect the TBH25P5R6.
At last if I would like to tune the capacitors, how do I measure Ls and LS'. I have been trying to figure that out but i can't understand what exactly needs to be exited with 1V RMS 100Khz?
Kind regards,
Adrian