This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The voltage waveform at coils of bq500412(Transmitter) and bq51020(Receiver)

Other Parts Discussed in Thread: BQ51020, BQ500412, BQ500110, BQ51013, CSD97395Q4M

Hi all,

Would you mind if we ask voltage waveforms which are at coils of bq500412(Transmitter) and bq51020(Receiver)?

Our customer asked us about  voltage waveforms which are at coils of bq500412(Transmitter) and bq51020(Receiver). But we don't have bq500412's EVM and bq51020's EVM.

We only have bq500110's EVM and bq51013's EVM, and we measured voltagewaveforms at coils using these EVM.
(Please refer to attachmentfile)
2046.Attachmentfile.pdf

So, when we use bq500110's EVM and bq51013's EVM, voltage waveforms at coils(receiver and transmittr) are similar to Attachmentfiles'one , or not?
Please let know us.

Kind regards,

Hirotaka Matsumoto

  • Hi team,

    We posted these question two weeks ago.
    However, there is no reply.
    So, if you don't have answer, please let know us.

    Kind regards,

    Hirotaka Matsumoto

  • Yes the bq500412 TX and bq51020 RX waveforms will be similar to those see on the bq500110 TX and bq51013 RX.

    The bq500110 waveform in the scope capture is at the TX coil (L2) and capacitor junction.  Both the 110 TX and bq500412 TX have similar power sections driving the TX coil, half H-Bridge.  But note that the 110 TX is a 19V input and 412 TX is a 12V input system, TX coils and resonant capacitor configurations are different.  Expect some differences.

    The bq51013 waveform in the scope capture is AC1 and AC2 input to the RX IC.  The two pins feed a full wave rectifier inside the IC, output is RECT pin.  The bq51020 will use a full wave rectifier also and output will be at RECT.  The 020 RX will use an improved synchronous rectifier to increase efficiency.  Again expect some differences.

  • Hello Bill san,

    Thank you for your help.
    If we need some information of bq500412 and bq51020, we don't hesitate to contribute on this forum. 


    Kind regards,

    Hirotaka Matsumoto

  • Hello Hirotaka,

    I am in need of the input waveforms to the coils for bq500412. Would you happen to have the exact waveforms ? 

    Or the PWM input and VSW output to and from the synchronous buck nexFET power stage (CSD97395Q4M)

    I look forward to hearing from you. 

    Kind regards,

    Kanav Batra