Hi,
I recently had my receiver based on bq51050b receiver IC set up with a transmitter based on bq500212A transmitter.
when i move the receiver close to the transmitter i can see the LED on the receiver board goes on and the green LED on the transmitter starts blinking (indicating power transfer). with the help of a multimeter i can see the current delivered to the battery is about 500-600 mA ( the value isnt an issue for me right now) but this lasts for few seconds then the red LEd on the transmitter starts blinking for few times then it turns on and the power transfer is shut down; this continues to be repeated again and again . sofar i havent been successful in having a constant charging current and it seems like the receiver is getting power with every blink of the green led on the transmitter side ( when LED is on the battery is charging and when the LEd is off the current goes to zero). I would like to have some help on this issue.could this indicate a problem with the receiver side or something else? right now i dont have another receiver to test with but i'll try to have one soon.
i have attached the receiver side schematics ; any comments or thoughts are highly appreciated.
Thanks,
Mahmoud