Dear TI wireless power support staff,
We are designing a product that features the BQ51013B IC to charge a battery. Currently we are testing one prototype with a known good TX. Our prototype uses the Mingstar 312-00015 coil and after tuning it we find it difficult to connect to the TX station, however after finding a "sweet spot" it just connects, works fine and fully charges the battery without interruption. I was wondering if COMMx capacitors may have an influence in this issue since another prototype we tested had 22nF COMMx caps and in this prototype we switched to 47nF COMMx caps.
The first prototype with 22nF COMMx caps connects easily but will not charge properly. (This one had the coil detuned)
The tuned-coil prototype with 47nF COMMx caps will not connect easily but charges properly without interruption. This one features 57nF as series coil caps and 702pF as parallel coil caps.
Thanks for your advice,
Luis.