Hi,
We are working on a device that will incorporate wireless charging. We are using BQ500212A for the transmitter and BQ51050B for the receiver. Our schematics are all based on the evaluation modules. The charging receive is incorporated into our device that also contains microcontroller, wireless module, and other components. The battery we are using is an 1850mAh lithium-ion rechargeable battery, and our device draws about 180mA current.
A problem we are seeing happens after the battery drains to the point where device shuts off. After this occurs, when we put the device with charging receiver onto the charging transmitter, the device does not boot up properly. The battery appears to be charging, but the microcontroller and wireless module are not functioning properly. We would then have to unplug and plug in the battery again (while the device is on the charging transmitter) for everything else to boot up.
I probed the battery input pins, and I’ve attached the oscilloscope shot of the battery boot up effect:
When I placed the device to charging, this is when the battery ramps up, as shown in the attached picture. But there is a saw-toothed ripple happening for 10ms before the voltage reaches the full 3.3V. I am thinking this is what is causing the other components to not turn on correctly.
I tried increasing the current limit, Ilim, to 1.4A (originally at 1A), but this still does not fix the drained battery boot up problem. The battery and the charging receiver chip got really hot instead.
What could be causing this? Are there settings on the BQ51050B chip that deals with this?
Thanks for the help!