hi:
i use the bq51050 .
the conditions are below:
1.Charging current is 150mA
2.The RX AND TX distance is 15mm.
when i charging the battery,i had auto recovery in TX sometime,
I adjust the termination resistor from 5k ohm to 1k ohm.
i can not see the phenomenon.
i check the BQ51050 Datasheet.it means"Note that this packet does not turn off the transmitter and is only used as an informative indication of the mobile device’s charge status".
is it correct?