Hello,
We are designing a wireless power system with the BQ51050B for a small wearable device. We have selected a coil which TI have also used in the tests for the reference design (see TIDA-00329 Test Report). The coil is Wϋrth 760308101303. We have calculated C1=56nF and C2=560pF for the capacitors in the resonant LC circuit. The system was tested with a TI TESLA transmitter, but we are getting extremely small working distances. If plastic is inserted between the two coils the receiver fails to start up. Can you share the values you used for the tests in TIDA-00329 with the same coil? What working distance did you achieve with that coil?