Hi.
I use the USB INTERFACE ADAPTER to control frequency shift with the BQ500414-EVM and our BQ500414 board.
I put the RX(51013B-EVM) with no load on the TX.
It's frequecny is 160Khz,I set the frequecny to 190KHz.
But it can not change the frequecny from 160kHz to 190KHz,
But I push the TX(ON/OFF) buttom,the TX be turned off.
Both BQ5004141-EVM and ourBQ500414 are the same.
so the communication is ok with TX(BQ500414).
What's wrong with the frequecny shift application?