Hello,
I have a very small single cell LI battery with a fast charge current rated at 6mA. Can the BQ51050 support this low of a charge current?
Thanks,
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a very small single cell LI battery with a fast charge current rated at 6mA. Can the BQ51050 support this low of a charge current?
Thanks,
Jason
Dick,
Thank you very much for your quick replies and the suggestions. I think I will go about minimizing the TIDA-00318, but I have a few questions.
Once again thank you for your quick replies and advise.
Thanks,
Jason
Dick,
My understanding of your response to my first question is that in the article you have a system with no feedback ("Open loop") and the output will be directly influenced by the frequency as you mentioned. Closed loop, in the TI chipsets case, is the dynamic efficiency scaling which effectively moves a system too and from resonance at 100kHz to achieve the appropriate Vrect based on current out.
Is there a way I can utilize this open loop system to help design an appropriate Rx?
For example, a problem I have encountered with past Rx is that the system was operating constantly around 205kHz, which I believe is a problem of L2 having to large of a value. In the article, they used the open loop system to find a Vrect value at a desired frequency, in the paper 5.15V at 150-160kHz.
Why did they use 19Vpp as the AC input? Could I use 19Vpp input to help design a system that meets my Vrect and Frequency requirement?
Thanks a lot,
Jason
Dick,
Thank you very much for answering all my questions! I have one final question. I just created a BOM for the TIDA-00334 on digikey and I have run into a problem with a missing TI component. On the BQ500212AEVM-550 there are two CSD97376CQ4M NexFET Power stages. On the TIDA-00334, I am guessing there is not enough room, so seperate components were used. I am trying to find CSD25302Q2, which is a MOSFET, P-CH, -20V, -5A, SON 2x2mm. It seems like it has been discontinued, I cannot find it on the TI website, Digikey, Mouser. I even tried to find substitute parts with the same footprint, but no luck. Could you help me with find a replacement part or lead me in the right direction?
You have been immensely helpful.
Thanks,
Jason
Hello Jason
You have a couple of options for the power section on the TIDA-00334.
1.) Low cost logic drive used on the TIDA-00334---replacement for CSD25302Q2 is the CSD25310Q2 (same footprint) and Mouser has them in stock. I will update Sch and BOM in the next few weeks to show this and fix other bom issues.
2.) Small integrated solution using CSD97376CQ4M---Design used on the bq500212A EVM, it can be used here also.
3.) MOSFET Drive solution using TPS28225—Design used on the bq500211 EVM. This driver has worked very well for us with no problem. Any number of external N-type mosfets can be used but the lower the RDSon the better.
Also I have other small TX designs in work.
Sonoki-san,
The charge current will regulate well at 200mA to 300mA. The termination current has a wide distribution at low currents. If the user sets the termination current to 20mA, there may be a wide distribution of actual termination. For a small sample size, the results may be very good, but as the number of devices increases, there will be an increased likelihood that there will be a wide spread in termination current. We do not spec the termination at that level, but I would expect actual termination currents to possibly range from 10mA to 30mA.
Let me know if you need further clarification.
Regards,
Dick
Hi Dick,
Thank you for your quick response. I understand we need to care about distribution of termination current. And also I understand that the possibly range of termination current will be from 10mA to 30mA, then can you please let me know the guaranteed minimum termination current? Is it 120mA as attached?
Best Regards,
Sonoki
Sonoki-san,
The bq51050B will terminate, the concern at lower currents is only the accuracy of that termination current.
Regards,
Dick